No compromise on safety
Safety clothing according to EN 20471
High-visibility clothing is legally required to be worn in certain working conditions. People working in road construction, for utility services, as couriers, refuse collectors or on runways are obliged to wear high-visibility clothing. High-visibility clothing is also needed in road traffic, rail transport, emergency services and the police. Higher visibility will provide greater safety in dangerous situations. The wearer must be noticeable and seen under all circumstances –- both during the day and at night. Some NEON line products from Würth MODYF also meet UV standard 801. These certified products protect the body from sunlight and prevent burning of the skin.
The standard defining which garments provide sufficient visibility is EN 20471. The internationally recognised standard distinguishes between three protection levels. The higher the risk in a particular work situation, the higher the safety class must be of the high-visibility clothing.
Supplementary information on the correct handling of high-visibility clothing:
- High-visibility clothing sets must always be worn in their entirety.
- High-visibility trousers must not be shortened or rolled up. The distance between the ground and the first reflective strip is prescribed.
- High-visibility clothing can be washed a limited number of times. Note the number specified on the label.
- Several garments in combination result in a higher safety class. This requirement is met based on the visible area when worn together. The highest achievable safety class for high-visibility clothing is protection class 3.
This means, for example: Jacket protection class 2 + trousers protection class 2 = entire outfit protection class 3
More comfort and protection with the latest technologies
From E-CARE technology to ODOURSTOP - Workwear from Würth MODYF is equipped with the latest textile technology. Learn about the properties of our workwear below:
E-CARE: 99 % protection
Smartphones are an indispensable communication tool in today's world. We are exposed to constant radiation through Wi-Fi, Bluetooth and 4G/LTE. E-Care technology protects your body from electromagnetic waves and thus from harmful radiation. The E-Care material is certified according to the OEKO-TEX® 100 standard. The fibres form a barrier and prevent the transmission of electromagnetic signals to the body.
SILVERPRO: Intelligent textile
Every person feels climate differently, as we all perspire or perceive cold at different thresholds. The reflective, silver dot design regulates body temperature for maximum comfort. Body heat is reflected and is therefore maintained. Body moisture, such as sweat, is transported to the outside by the functional fleece material.
ODOURSTOP: Always stay fresh
A highly innovative and antibacterial textile that ensures odour control and thus lasting freshness. The growth of bacteria is stopped and prevented. The natural silver salt quickly and reliably neutralises sweat odour.
MODYTEX: Stay dry when it gets wet
The processed functional membrane is waterproof and yet breathable. This high-tech membrane is used in a wide variety of Würth MODYF products, both in work clothes and in safety shoes.
FAQ - the most common questions on fabric choice and cleaning
What material should my work clothes be made of?
Every material has its advantages. Cotton is skin-friendly and offers excellent comfort. It does not melt (e.g. in the case of flying sparks), is durable and very absorbent. Polyester/cotton blended fabric is characterised by being easy to care for and very durable. It dries quickly and does not shrink when washed.
Why do colours sometimes fade more in the wash and sometimes less?
Different fabrics have different properties. Cotton for instance is not as colourfast as polyester. Using colour liquid detergents is likely to preserve the colours for longer. All-in-one detergent bleaches out the colours.
How do I get my laundry germ-free?
Germs on fabrics are not reliably killed at low washing temperatures. This only occurs in washes at 60 degrees or above. If this is not taken into account, germs may become established, which often brings unpleasant odours. So that you no longer need to worry about keeping your work clothes at their germ-free best, Würth MODYF has created the Cetus Collection. Not only is the collection non-itching, OEKO-TEX® 100 certified, durable and metal-free, it can also be washed at 60 degrees.
How do I best care for my embroidered or printed work clothes?
To ensure that you can enjoy your work clothes for a long time, please observe the care label on your Würth MODYF clothing.
The Adolf Würth GmbH & Co. KG collects and processes the personal data provided in the form in order to process the requested request for you. Please note the mandatory fields in the forms. The legal basis for this processing, the absolutely necessary data, is Art. 6 para. 1 lit. b GDPR, implementation of a pre-contractual measure. The processing of data voluntarily provided by you is carried out on the basis of Art. 6 para. 1 lit. f GDPR. Thereafter, processing is permissible which is necessary to safeguard our legitimate interests. Our legitimate interest is to have contact with you, our customers, to improve our consulting quality and to be able to contact you more easily in case of possible queries. The data collected will only be stored by us for as long as is necessary to process your enquiry and to contact you. They are then deleted.
Supplementary data protection information, in particular regarding your rights to information, correction, deletion, restriction of processing, objection and complaint, can be found in our data protection declaration.